Download the Photonic Applications Package Manager from the Photonic Applications Package Manager download site.
Unzip the downloaded ZIP file and run the EXE file with administrator privileges. The following screen will appear. If you do not run it with administrator privileges, errors may occur during software package installation, and the installation may not complete successfully.
Follow the steps below to install the software:
In many cases, measurement instrument control software requires other software to function properly. Software dependencies will be indicated in the Package Manager. First, install the instrument control software you want to use, and then install the software marked with an arrow icon as shown in the figure below.
Additionally, during installation, you may be prompted to install other dependent software first. Carefully read the messages before clicking OK to proceed with the installation.
After installation is complete, launch the software from the Windows system. You cannot launch the software from the Photonic Applications Package Manager.
If the message “Error! Can’t initialize plug-ins directory. Please try again later.” appears, restart the Photonic Applications Package Manager with administrator privileges to resolve the issue.
In environments without internet access, the Action column may display “not available” in light gray, preventing package file downloads. In this case, download the package files on another device and add them manually.
Click “Download folder” at the bottom of the window. By default, this opens the folder: C:\ProgramData\Agilent\Photonic Application Suite\Download
Inside this folder, the Packages folder is the storage location for package files.
Place the package files (ZIP files) downloaded on another device into the Packages folder. There is no need to unzip the ZIP files.
After copying the files, click the refresh button to the right of the Action column. If the Action column changes to “Install”, the addition is complete. Click to proceed with the package installation.